Hi TI Expert
I have an over heat problem in LM2936MP-5.0 When the external power is 30 V.
The load current is below 30 mA.
Regards
Ihab
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI Expert
I have an over heat problem in LM2936MP-5.0 When the external power is 30 V.
The load current is below 30 mA.
Regards
Ihab
Hi Ihab,
What's the output voltage of the LDO and in what package? When you say heat problem, did the regulator hit thermal shutdown?
Regards,
Jason Song
Hi Jason
The output is 5V in package LM2936MP-5.0_NOPB ( SOT-223).
the heat problem by hand touching , It is too hot that you can't touch it,
We should consider that there is a packaging stage and it will be hotter
Regards,
Ihab Alsheikh
Hi Ihab,
The LDO has a recommended junction temperature of up to 125C. I would not recommend using your finger to sense the temperature. Instead, please use a thermal gun or estimate the temperature by using (Vin-Vout)xLoadx Rja, the Rja for SOT-223 is 59.6C/W.
Regards,
Jason Song
Hi Jason,
Thank you for your replay.
(Vin-Vout)xLoadx Rj
(Vin = 30 V, Vout = 5V , Load = 30 mA)
that means the estimated temperature of LM2936 is 44.7.
adding the ambient temperature (40 C) which means 84.7 C. am I right?
The board which I used will work all the day, Could I face a problem because of regulator heat ?
Regards,
Ihab
Hi Ihab,
Yes, your calculation is correct. The LDO is designed to operate under 125C and you are good.
Regards,
Jason Song