This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25085-Q1: LM25085-Q1

Part Number: LM25085-Q1

Dear ,

i use LM25085-Q1 to build one DC-DC , 15V,18-25V input, and when output current larger than one current( 2A for example), the drv will keep low for hundred us, and FB pin thus abnormal cause of the ripple injected.

 drv, and FB signal(abnormal and normal both)as listed below. i tried to update the injected RC, but seems no change. do you have similar waveform before, seems strange, any advice on the root cause?