This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76925: VCOUT is clamped at 2.2V

Part Number: BQ76925

Hy, TI experts,

We use REF_SEL=1 (0.6 cell voltage gain) settings, and find that VCOUT can't go higher then cc. 2.2V, so we can't measure correct voltages above 3,8V

Using REF_SEL=0 it is working.

I also have to note that changing REF_SEL sometimes doesn't have effect. A long time power down needed before initializing the REF_SEL 

May be the device demaged?