We're wondering if the safety timer for this device can be set for a value higher than 10 hours with the use of capacitor values larger than 0.11uF. If so, what is the limit for the overall safety timer?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We're wondering if the safety timer for this device can be set for a value higher than 10 hours with the use of capacitor values larger than 0.11uF. If so, what is the limit for the overall safety timer?
Thank you
Hello,
The maximum supported safety timer upper value is 10 hours as specified in the datasheet.
Thanks,
Mike Emanuel
Please click "Resolved" if this answered your question.
Hi Mike,
What exactly is the reasoning behind this limitation? All I'm seeing in the datasheet is that the 1-10 hour range is simply "verified by design", which to me indicates that these ranges aren't necessarily based on testing or physical limitations. Due to other requirements in our system, we may not be able to charge in less than 10 hours, but would still like to have the added protection of a charge safety timer if possible.
Thank you
Hello,
As stated previously, the maximum supported safety timer setting is for 10 hours. At the time the part was released, most customers could charge within 10 hours. Some of our parts offer the ability to count the 10 hour clock at half the rate if you are in thermal, input voltage, or input current regulation.
What type of features are you looking for in a charger? I can point you in the right direction.
Thanks,
Mike Emanuel
Please click "Resolved" if this answered your question.