Hi,
I have a problem with BQ27441. Chip is implemented in a device and works good months. But suddenly BQ27441 go to state when it doesn't answer to i2c. In this case I must disconnect from battery and reconnect.
In datasheet I saw in Shutdown mode the chip can behave like this, but I haven`t sent the device to shutdown mode. Is it possible that the chip goes to Shutdown mode automatically for some reason and doesn't exit from this state? I don`t connected GPIOUT pin to the microcontroller and because of that I can`t get out the chip from this mode.
It is only my theory that this happens due to shutdown mode can it be anything else why the communication on i2c fails between the chip and MCU (restart MCU not helps, other devices on i2c are working properly... only BQ27441 doesn`t answer on i2c)
Please help,
thank you