Part Number: TPS560200-Q1
Hi
I aim to use the TPS560200-Q1 in design to get 3.3V max 400-450mA during peak Wifi TX, otherwise less then 100mA. My Vin will be 12V
This is my design, i have not yet done PCB layout.

I prefer to keep my BOM as universal possible, therefore, would there be any issues using the following components:
10 uF Inductor -> LQH43CN100K03
10uF Capacitor 0805 ->CL21A106KOQNNNG
This is the PCB layout
I await your reply
Thank You