Other Parts Discussed in Thread: BQ76942
Hello,
I am trying to figure out how accurate the BQ76952 temperature sensor inputs are without performing calibration.
I am using a 10k NTC (TDK NTCG163JX103DT1S, ±0.5% resistance, ±0.7% B-value). I have configured the BQ inputs to use the internal 18k pull-up resistors with NTC coefficients defined using TI's bq769x2 Family Thermistor Coef Calculator Tool (attached).
Without doing any calibration, I am seeing a pretty high temperature measurement error (~90C where my reference sensor is 68C). I was expecting it to be much better than this based on the datasheet information that the internal pull-up resistors are factory-measured.
What is the maximum expected error I should see using the uncalibrated temperature sensor inputs?
bq769x2 Family Thermistor Coef Calculator - NTCG163JX103DT1S.xlsx