Other Parts Discussed in Thread: TPS61030,
Hi,
Im designing a circuit for a project that im doign in my university witch is a thermometer with opamp signal conditioning connected to a arduino. Allthough its not asked of us im planning to take it a step forward and incorporate the thermometer in a portable data logger that is kinda usfull for a famaly member that need an equipmente like this.
For this perpouse i need a power supply circuite that is able to supply 5v to power the atmega328P and +-15V to power the opamps (and the +15V for the wheatstone bridge).
As im still a begginer in this and i dont have the means to do a teste circuite in a breadboard im asking if anyone could take a look at the the circuite ive planned to power the above mencioned project.
To recape i have designed:
-5volt input usb/solar pannel so charge li ion 3.7v battery(using the tp4056 with protection ic to do this)
- +5V to power the atmega328p(using the TPS61030)
- +-15v to power the opamps(with min of 150mA)(using the TPS65131 with is input connected to the output of the TPS61030)
- main power source li ion battery 3,7V.
I Apolagize in advance for my spelling mistakes,
and thank you for helping.