Hi,
I am testing the below circuit with 24V Power Supply.
My requirement: 3.3V @ 2A..

I have 2 Difficulties as below:
1. With a Load of 2.5Ohm, I am drawing 1.3A yielding 4.4W power. However, the regulator shuts down after 10seconds with No Output..
(However, if increase the load and draw about 1.2A, Regulator is working fine with no Shutdown happening..
2. With 24V/3A power supply, LMR33630 doesn't turn-on with a load to draw 1.2A. However, with 5A power supply, LMR33630 turn's-on with a load to draw 1.2A.
Does this mean that LMR33630 has a big inrush current that needs to taken care of.. If so, please advise how to do...
Thanks