This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR33630: Load Test

Part Number: LMR33630

Hi,

I am testing the below circuit  with 24V Power Supply.

My requirement: 3.3V @ 2A..

I have 2 Difficulties as below:

1. With a Load of 2.5Ohm, I am drawing 1.3A yielding 4.4W power. However, the regulator shuts down after 10seconds with No Output..

(However, if increase the load and draw about 1.2A, Regulator is working fine with no Shutdown happening..

2. With 24V/3A power supply, LMR33630 doesn't turn-on with a load to draw 1.2A. However, with 5A power supply, LMR33630 turn's-on with a load to draw 1.2A.

Does this mean that LMR33630 has a big inrush current that needs to taken care of.. If so, please advise how to do...

Thanks