This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7B81: GND(4) not connected

Part Number: TPS7B81

Customer's original board was designed for TPS7A6650QDGNRQ1. Due to shortage, they are trying to build boards using TPS7B8150QDGNRQ1 instead.

The difference is Pin 4, where TPS7A66 is CT pin, while TPS7B81 is GND. This is left floating on existing PCB.

Question:

Can TPS7B8150QDGNRQ1 work if Pin 4 (GND) is left floating?

Customer expects that the other 2 GND pins (Pin 5 & Pin 6), and Thermal pad are internally bonded with Pin 4, such that TPS7B81 would work without Pin 4 connected.