This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61196: TPS61196 400mA Continuous Current at only one Output

Part Number: TPS61196

Hello

The maximum continuous current is 200mA acc. to datasheet. The pulse current is 400mA per channel. What about the situation where I need 400mA continuous current, but only at one output and the other outputs are disabled. As soon as 2 outputs need to be active at the same time the current per channel would be 50% PWM of 400mA.

So is the limit at continuous 200mA because of the overall device heating when all channels are active or is every single channel limited to 200mA continuous?

Thanks for your help