Hi,
I have a question about the IoL on the RESET pin.
Customer request: Under the following conditions
Operating temperature: -10 ° C to + 60 ° C
VCC: 12V ± 1V
They need an IOL value that the VOL of the RESET pin is less than 0.6V.
According to Figure 3, 1.5mA or less is likely to meet this requirement.

This was my advice for the customer, but it was rejected because it was not a guaranteed value.
Can TI offer a guaranteed value?
This question is just to determine the pull-up resistance value of the RESET PIN.
Please tell me the recommended value of TI or how to decide it according to the customer's condition.
Best regards,
Hiroshi