Hi all,
I got four questions about this IC. Can you answer to those questions?
- In master IC, is spread spectrum enabled on the signal from SYNCOUT?
- In the datasheet, there is a statement "When the LM5143-Q1 controller detects 16 missed switching cycles, it enters standby mode and switches to a low IQ state to reduce the current drawn from the input" in datasheet 8.4.1. Can you tell me what "16 missed switching cycles" are? Is it the time < minimum on time?
- Regarding to 2, can you tell me what is the condition to exit standby mode?
- There are two types of standby mode, standard and ultra-low Iq. Does the device first enter standard standby mode and then ultra-low Iq mode? Or does it directly enters ultra-low Iq mode when MODE=AGND, so that standard standby mode is not used when MODE=AGND?
Thanks,
RYO