This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3897: delay time calculation

Part Number: TPS3897

Hello expert,

Customer has two questions about TPS3897 on the delay time setting. According to datasheet equation (2), it seems like it is not match about below table value. And also, do we have maximum delay time limitation? Customer is testing with 2*0.047uF and power on is fail. Could you kindly help on this case? Thanks a lot!!

Best regards,

Ann Lien

  • Hi Ann,

    I have check the equation and compared the typ value in the datasheet and both values matches.  This is how I calculated the time:

    tpd(r) = (0.047 * 4) + 40uS = 188.04ms.

    The equation requires the capacitor value to be in uF and the customer may be mistaken by using (0.047 * 10^-6) instead of just using (0.047).

    I need to look into the max delay time limitation so I ask for your patience.

    Ben

  • Hi Ann,

    According to the validation data, the max delay time limitation is around 12 seconds or about 3uF.  The result was done only at room temp.

    Ben 

  • Hi Ann,

    If I have answered all of your questions, please click on "resolved" to close the thread.

    Ben