Part Number: TPS2662
Other Parts Discussed in Thread: TPS1663,
I am working on a safety circuit where I need to essentially limit power, not just current.
I have experimented with adding a small voltage via a large resistor to the ILIM pin (along with the ILIM resistor) to cause the current to go down with higher input voltages so that you get the effect of a power reduction. The small voltage is scaled from the input voltage in order to stay within the 1V range of the ILIM pin.
If I do this just right, it looks like I can almost get to a constant power out (limit) regardless of input, which is what I desire.
In order to predict this effect reliably, and more importantly, involve tolerance that is more than just my ILIM resistance, it would seem that maybe I need to know the tolerance of the internal 1V that is controlled on this pin.
Or if you can supply a simple spice model that involves the tolerance of the set current that would also help.
Or an overview of where the TMR2662 current set tolerance comes from...like is it the scale factor (gain) variance on the 6632 term in the I=6632/Rlim term, or is it more related to the tolerance on the 1V held across Rlim or some of both...etc.?
Thanks
Glen