Hi Team,
my customer is using a small resistor in series to the bootstrap capacitor (EMI) of the TPS560430YDBVR. Is there a upper limit for the maximum allowed value of the resistor e.g., 100 Ohm?
In the datasheet it is mentioned that the capacitor type should be ceramic X7R with a value of 100 nF and > 16 V. Does also exists a range of the capacitance
in which the full functionality of the step down convert is guaranteed e.g., 47 nF .. 220 nF?
Thanks,
Obinna.