Part Number: BQ78350-R1
Other Parts Discussed in Thread: BQ78350, BQSTUDIO
Hi,
we log the data comming from the BQ78350 chip and there we have seen, that some times we get wrong values from the BQ chip. Previously I thought it is because we are reading to much data, but I tried to read with more than 1000 messages/s and the only thing I get are timeouts (10ms), because the chip is anymore able to handle it. This is fine, but I don't see any problem when a wrong value occurs. It does not matter on which parameter, they occur on temperature, voltages, currents ...
Is there something else which can lead to wrong value readings?
Wrong voltages


Wrong current value

Here are more issues