Hello TI experts,
I need to use the device to charge a 10A/h Li-Ion battery pack using the P-Channel MOSFET configuration as per datasheet. As the requirement is a 2A / h charge rate, instead of searching of 'extreme' mosfets and also because we have not so much space for thermal dissipation ( it is an handheld device ), I was wondering if i could use a couple of more common MOSFET's connected in parallel... Is there any concern about such a configuration...?
Thanks in advance for any reply...
Regards
Alex