Hi, I did charge/discharge cycle for standard single AA NiMH 2300 mAh cell, unfortunately the tool does not recognize the NiMH chemistry at all...
in the attachment you can fin input and output files
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, I did charge/discharge cycle for standard single AA NiMH 2300 mAh cell, unfortunately the tool does not recognize the NiMH chemistry at all...
in the attachment you can fin input and output files
Hello,
The chem ID matching is for the voltage correlation, so it will find any chemistry ID that matches the discharge profile. I would recommend reducing and IR and connection losses as much as possible and run the test again, usually we wan the error under 5%.
Sincerely,
Wyatt Keller