Other Parts Discussed in Thread: BQ27541
您好!
请教BQ27541-G1在40°C工作环境下,外部NTC温度检测到的温度是-33°C,芯片内部温度检测到的温度是-40.2°C,请教怎样解决外部NTC温度检测不准的问题?(已经排除了芯片本身,NTC(10K,3435,1%),校准(无法校准,提示超出范围)这些问题,原理图和外围元件按照芯片规格书的电路)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
请教BQ27541-G1在40°C工作环境下,外部NTC温度检测到的温度是-33°C,芯片内部温度检测到的温度是-40.2°C,请教怎样解决外部NTC温度检测不准的问题?(已经排除了芯片本身,NTC(10K,3435,1%),校准(无法校准,提示超出范围)这些问题,原理图和外围元件按照芯片规格书的电路)
Hi,
Is the environment temperature 40°C? If so, internal temperature should be 40.2°C, not -40.2°C. Please measure NTC resistor to make sure it is working correctly.
Best Regards,
Abraham
Hi,
BQ27541温度传感器模型为Semitec 103AT,-40C时对应电阻为188.5K。后续支持请移至中文技术论坛: https://e2echina.ti.com/