Hi Team,
Customer is using BQ76952 and did a 12S BAT pack prototype, but during the short-circuit testing they found a issue that:
- At short circuit status, BQ76952 DSG voltage will change to ‘High’ automatically ~every 6ms, which may cause the MOSFET be broken.
- If short circuit protection be trigged, BQ76952 will change from ‘SEAL mode’ to be ‘UNSEL mode’ itself.
- Enclose please also refer to the gg file and log information (bqz firmware version is 0.36).
Attached is related part's schematic, log date & gg file, also the testing waveform as below, could your kindly check it and suggest what’s the potential reason & further experiment to verify the root cause?
![]() |
![]() |
CH1: of DSG_FET CH2: of DSG_FET of DSG_FET of BQ76952 |
CH1: of DSG_FET CH2: of DSG_FET of DSG_FET of BQ76952 |