Other Parts Discussed in Thread: LM5069
Hi Sir:
in slva833d, for a 24V system , the max IN-OUT voltage during surge test is around 60V (Figure 4-4,When a ±500 V, 2Ω surge pulse is applied, the input
voltage clamps to a ±44 V maximum. The Internal FET experiences maximum stress during the negative surge event. Maximum voltage across the device is the sum of the input clamp voltage and the output voltage under no load conditions. The maximum device stress at nominal), which is close to max rating of TPS2660;
how do we do Surge Protection for 48V input system?
thanks a lot
Sean