Part Number: LM25066A
Hi Team,
The customer wants to confirm whether LM25066A can use the program to shut down the chip? What do we need to do if we can?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM25066A
Hi Team,
The customer wants to confirm whether LM25066A can use the program to shut down the chip? What do we need to do if we can?
Hi Yadong,
Thanks for reaching out to us. The device can be enabled or disabled by writing 80h or 0h to the OPERATION (01h) register respectively. The OPERATION command is a standard PMBus command that controls the MOSFET switch. This command may be used to switch the MOSFET ON and OFF under host control.
| VALUE | MEANING | DEFAULT |
| 80h | Switch ON | 80h |
| 00h | Switch OFF | - |
Please click "This resolved my issue" button if this post answers your question.