This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ20Z95: Hardware vs software Overcurrent Protection Levels

Expert 4640 points

Part Number: BQ20Z95

Dear Support,

Could you explain the architecture difference of the Hardware and the Software OCP levels (described page 18 of the Tech Reference)?

Regards,

  • Hello,

    Software based controls use measured values (current in this case) to run the comparison on the real current with the set threshold programmed in.

    Hardware based protections usually use comparators and a bit selection to apply different reference voltages to the comparator, hardware protections are much faster because of this.

    Sincerely,

    Wyatt Keller

  • Hello,

    As the hardware protection thresholds (AFE protection) are adjustable by writting a value in the dataflash, Does it means that the hardware protections (AFE protection) are software dependant ? 

    The dataflash lifetime indicated in the datasheet is 10 years. Does it means that after 10 years, the threholds set for the AFE protection could change ? In that case, does the AFE protections are still valid ? 

    Thank you

    Regards

  • Hi Wyatt,

    Could you come back on the two points above, from Mr Froger?

    In addition, is there a way to get the dataflash recovered by reprogramming it after 10 years?

    Regards,

  • Hello,

    Sorry for the late response.

    The bit settings set the comparator voltage values for the hardware protections, so in a way it is based on settings in the dataflash.

    The minimum is 10 years and 20,000 cycles. If the data has become corrupted there would be no way to recover the original memory.

    Sincerely,

    Wyatt Keller

  • Hello Wyatt,

    Thank you for the feedback. That answer my question. 

    Regards,

    Mathieu