Hello TI Team!
Have a nice day! Hope all are well and safe,
We are using BQ76952 in our BMS design(14S2P, 330WH, o/p voltage- 48-57V, max charging current -7A, max discurrent-20A). We have some question regarding BQ76952 power modes that need to clear during our designing,
Please provide answer of my queries as soon as possible
Power mode queries are mentioned below,
1. If there is no charging and discharging then How much time that device will be remain in normal mode before switching to sleep mode?
Can we configure this time period?
2.If there is no charging and discharging then How much time that device will be remain in normal mode before switching to deep sleep mode?
Can we configure this time period?
3.How much time that device will be remain in sleep mode after switching from normal mode?
Can we configure this time period?
4.How much time that device will be remain in deep sleep mode after switching from normal mode?
Can we configure this time period?
5.How much time that device will be remain in deep sleep mode after switching from sleep mode?
6.Given condition to switch normal mode to sleep mode mention in datasheet is that
if CC1 current < Current threshold [Power: Sleep: Sleep Current] then we want to know that
(a)After how much time it will test this condition in normal mode periodically?
(b)What is the value of CC1 Current need to switch in sleep mode from normal mode?
7.Given Condition to switch sleep mode to normal mode mention in datasheet is that
if CC1 current > Current threshold[Power: Sleep: Sleep Current] then we want to know that
(a)After how much time it will test this condition in sleep mode periodically?
(b)What is the value of CC1 Current need to switch in normal mode from sleep mode?
8.What is CC1, CC2 and CC3 current value (in Normal mode, sleep mode and deep sleep mode) and How does CC1, CC2 and CC3 current value calculate by device in given
following conditions?
(i) What is the value(CC1, CC2, CC3) in normal mode in if no charging and discharging, how does device calculate these values?
(ii) What is the value(CC1, CC2, CC3) in normal mode in if only charging, how does device calculate these values?
(iii)What is the value(CC1, CC2, CC3) in normal mode in if discharging, how does device calculate these values?
(iv) What is the value(CC1, CC2, CC3) in Sleep mode, how does device calculate these values?
(v) What is the value(CC1, CC2, CC3) in deep Sleep mode, how does device calculate these values?
(vi) can we any change in value of CC1, CC2 & CC3? if yes how?
9.Does CC2 & CC3 current value play in mode switching? if yes then how?
10.Does the device switch from sleep mode to deep sleep mode only by DEEPSLEEP() subcommand? or there is any time period after
after which device switch to deep sleep mode from sleep mode?
Does DEEPSLEEP() subcommand given by controller to device? How does device power up if it is in deep sleep mode?
11.Does I2C communication is possible with the BQ76952, if it is in sleep mode/Deep sleep mode?