Other Parts Discussed in Thread: PTEA415050
Hello Tech Support Team.
I have a question about PTEA415050 part which I am currently using in one of our brand new design.
We are using this component to convert the POE (Power over Ethernet) Supply which is 51V into 5V supply.
This 5V supply is then used to generate 1.2V/2.5V/0.67V/0.78V and is used by our device onboard.
It has been observed, that when the brick is enabled by connecting the Pin-2 to Pin-3 of this component, the EMI noise increased considerably and is injected into MDI lines of our PHY which are running nearby.
I wanted to know if this is a known issue with PTEA415050 and if there is any remedy to prevent this EMI noise from speading to the surrounding circuitry.
Is there any application note which describes how to prevent this EMI noise or something along the same lines?
Any help would be much appreciated.
Thanks
Shahab
408 457 7263