Other Parts Discussed in Thread: LM2576HV, LM2576
Hello,
I'm currently designing a adjustable supply for a power op-amp with a digitally adjustable output. The output will be regulated with a DAC and fed in via an op-amp to the reference pin. I designed a separate positive and negative rail with each a LM2576HV-ADJ. The positive rail for the op-amp wasn't a problem, but the negative rail causes trouble. I build the circuit as in the following figure LINK. The component values are the same as for the positive rail. When I turn the power the current rises and the output voltage doesn't reach the expected value of -35V. Are the components wrong or is there anything else I can to to make this converter work.
Thanks in advance.