This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compatibility between bq24190, bq24297 and bq25890

Other Parts Discussed in Thread: BQ24190, BQ24297, BQ25890

Hi Everyone,

Now our customer has evaluated bq24190 on thier test board, and now they would like to bq24297 and bq25890 also on the same test board, because we know that these devices are almost pin compatible though need to care 12pin and 24pin as attached. Then can they use the same external component circled red in attached schematic? Please let me know the component they need to change value.

Best Regards,

Sonoki / Japan Disty

  • The 0Ohm resistor is correct.

    All components in red have correct value. I would suggest to change PMID cap to 8.2uF which is commonly used for all three device.

  • Hi Sam,

    Thank you for your comments. I understand that bq24190, bq24297 and bq25890 can be used with the same external components though PMID cap should be changed to 8.2uF.

    Best Regards,
    Sonoki