Other Parts Discussed in Thread: BQWIZARD, BQ78PL114
If the "ship" bit is toggled and the battery pack is removed from the SMBus, the battery goes to low power mode immediately and all FETs switch off and stay off correctly.
If the "ship" bit is toggled and than the "safe disconnect" feature of the bqWizard is used and the battery is disconnected, the FETs stay switched off only approx. 2 minutes. During this 2 minutes, two RSOC LEDs are blinking. After this time, the FETs are on again.
How is it possible, to enable low power "ship" mode and use the "safe disconnect" feature?
Regards
Andreas