I scanned the Simple Switcher forum, but the non-isolated DC/DC forum seems like a better fit.
I have -12 V ±5% on input and need a reasonably well-regulated +5 V output at a minimum of 1 A, preferably 2 A. I'd like to be somewhat efficient, so I'd like to avoid a linear solution. I also need to filter both directions so that my switcher does not create noise on the -12 V supply or on the +5 V output. The output will probably be easier to filter. I assume the input might need some resistance for isolation, which will understandably reduce efficiency. In that case, efficiency is not as much of a priority as low noise, so long as the efficiency is better than typical linear inverting supplies.
Any hints? I'm also hoping for low parts count, but perhaps I'm asking for too much?
p.s. I'd like to support input voltages as high as -18 V, although the -12 V 5% is most likely.