Other Parts Discussed in Thread: TL1431-Q1, TL1431
Hello,
I am designing a crowbar circuit that is supposed to activate in the event that the motors are running and a safety contactor opens and cuts power to the controllers. Vmax for the DC bus is 126V so I want to sense 110% of Vmax which is ~140V. I am leaning away from a regular Zener because of the temperature dependence and the 5% tolerances. This circuit cannot accidentally trip! I figured this shunt reference (TL1431-Q1) would work well, but I see the max cathode voltage is 36V. Should I add a large power resistor on the cathode line to drop the 90V so Vdd is 36V?
Thanks!