Hi everyone,
We are trying to do a H-bridge using UCC21520 and power mosfet STFW3N170 VDSmax 1700V -> datasheet.
There is a typical application in the datasheet to do a half bridge:
We didn't put Rds and Rdt, RoFF_A+Diode, RoFF_B+Diode.
The problem is that we are not able to trigger correctly the upper mosfet. The lower mosfet works well depending on INB's level.
The logical side is supplied with 5v, the driver's supply is separeted with 20V and the HighVoltage is 50V, the VSS of the HV and driver are conenected together.
It seems that when we put a 1 logic in INA we can see the bootstrap capacitor release its charge into the gate but it lasts like 1ms then the mosfet become locked again.
Should we put a resistive load in output anytime to have a small current through the output line?
I know that the Bootstrap capacitor + Diode are very important but I don't really understand how it should work is this circuit, we took a random value 1uF with 2.2Ohm to limit the current and a shocky diode rated for 600V
Thank you very much