Part Number: UC2842
Hi Team,
My customer is using our UC2842 in old product, recently they need to improve the protection feature, they hope to realize Hiccup mode when load shorted. I'm thinking that when output was shorted, as the auxiliary transformer and the auxiliary winding polarity is same, so the auxiliary winding voltage Vaux will be also pulled low, then our UC2842 will be shut down and startup again, like "Hiccup behavior". If so, that is what customer wanted! However, the reality is cruel.... When we measure the output of auxiliary winding output voltage and Vaux, it seems the Vaux is not pulled down due to that these is leakage inductance, so it seems Vaux is not pulled down.
Below are two waveform with normal load status and 5V output load shorted to GND:
When we add a 27 ohm series resistor+100pF cap to parallel with D2, it seems the Vaux will be pulled low when 5V output short to GND, thus seems realize the Hiccup mode. However the standby current will increase about 2W which can't be accepted by customer. More detailed schematic as below for your check:
So based on above information and description, can you or anyone give a available solution to realize Hiccup mode with our UC2842? The simple the solution the better, thanks a lot!
BTW, not sure how other customer realize the protection feature? Do you have something that can share with me, thanks a lot!
Best regards,
Sulyn Zhang