This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am developing Three-Phase Inverter Gate Drive circuit.
I design the Isolated IGBT gate drive power following TIDA-00199 reference design, but changing Zener diode "BZX84J-B15,115" to "BZX84-B15".
Schematic is down below:
The output of secondary side will got a strange ripple (about 1V).
C1 is the SW output of LM5160
C2 is the voltage between PB15 and PB-8 ( Measured by isolated voltage probe)
How can I reduce this ripple?
Does diode "BZX84-B15" cause this problem?
Thanks a lot
Yi-Lin
Hi David
Sorry for late reply.
I reduce C73 to 4.7nF.
I measure the SS pin of LM5160 and Vout(C80) on primary side.
The strange ripple exist on primary side.
Picture 1: Before reducing C73 to 4.7nF
Signal 1: Vout(C80) on primary side
Signal 2: SS pin of LM5160
Picture 2: After reducing C73 to 4.7nF
Signal 1: Vout(C80) on primary side
Signal 2: SS pin of LM5160
Yi-Lin
Hi David,
C79 and C80 are electrolytic capacitor, will this cause the problem?
I change C79 to 10uF and add a 22uF Tantalum capacitors on Vout of primary side
The ripple of Vout on primary side can be reduced
C1: Vout on primary side(C80)
C2: SW pin of LM5160
But sometime the LM5160 will be unstable, with multiple ON-time bursts followed by a long OFF-time.
I add a dummy load 2k Ohm resistor the primary side.
and the circuit works
Thanks a lot
Yi-Lin