This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5170-Q1: Single phase operation

Part Number: LM5170-Q1


Hi,

I'm using the LM5170-Q1 in a design for an MPPT, however the power level is only 200W so a single phase works fine. What do I need to do with the inputs and outputs of the second channel? Can I leave them floating or do they need to be tied to some particular nets? Also out of curiosity is it possible to implement some sort of valley switching when in DCM?

Kind regards,

Luc Does