This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5050-1-Q1: LM5050Q! Current Draw for Vin and Vout

Part Number: LM5050-1-Q1


I'm trying to determine the quiescent current draw of LM5050Q1MKX-1/NOPB while Vs (pin 1) is held at 0V while Vin (pin 4) and Vout (pin 6) are present (10V to 16V). The datasheet only specifies the various pin currents when Vs is enabled (set at Vin).

Please provide the current draw for Vin (pin 4) and Vout (pin 6).