Part Number: BQ40Z50-R1
Other Parts Discussed in Thread: BQ40Z50
Hi,
I have a similar problem as
.
That thread wasn't answered.
The only difference is that I use BQ40Z50-R1. Once BTP_INT is set, it can be cleared only by device reset, which is unacceptable for me.
I have updated the firmware to bq40z50_r1_ v1.06_build_36, but the problem persisted.
Is there any way to get this feature working right (i.e. set when the remaining capacity has depleted to a certain level, and clear when it is above this level)?
Best regards, Michael.