This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LT1054: the device is failed

Part Number: LT1054

To whom it may concern, 

I use the LT1054IP to convert +12V to -12V.  The +12V/-12V are used for the power of the OP amplifier.  I measure the current in the -12V circuit, the current is 14mA .  Sometimes the LT1054 will fail, the voltage will be 0.X V.  I think that the output current of LT1054 is sufficient for my load current(14mA).  Can you give me some advice? The attached file  is my circuit.  Thank you.