Dear Sir/Madam,
Can i know hat is the maximum current that can be "sourced at the same time" from this IC? Are the following and therefore, the system can deliver a total of 700-mA to the loads in total (Isw + IPMID +iLS/LDO = 700 mA)?
Best regards,
kpk