Part Number: LM1117
This voltage regulator is heating up at 100mA.
Any help/suggestions why?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Rony,
You are dissipating 700 mW in order to convert 12 V to 5 V at 100 mA. We can use the Thermal information table for the DCY package to estimate that the junction temperature will be ~43.12 C higher than your ambient temperature (0.7 W x 61.6 C/W).
If you wish to reduce the power dissipated in the LM1117, you can generate an intermediate voltage rail between the 12 V and the LM1117 by using either DCDC switching regulator (most power efficient solution for the system) or another linear regulator. You could also place a power resistor in series before the LM1117 input capacitor. This resistor would reduce the input voltage local to the LM1117 by 100 mA x the resistance; however, you would want to make sure that the resistor is rated for the power that you would be dissipating in it.
Very Respectfully,
Ryan