Other Parts Discussed in Thread: BQ76200
Hello,
I'm planning to use a hall effect current sensor at high-side instead of shunt resistors along with a op-amp to decrease output into SRP/SRN limits of bq769x0 for current sensing.
I think maximum measurable range of SRN and SRP pins of bq769x0 is 400mV, according to the datasheet.
Datasheet shows min and max typical for SRN and CCrange as -200mV, +200mV and for SRP as -10mV, +10mV.
So;
I'm planning to reduce the output of current sensor to -200, +200 range, but which pin should i connect it? SRP to ground and sensor to SRN?
Also I'm planning to use an external high-side nfet driver (bq76200) with seperate paths for charge and discharge. Should I use bidirectional sensor for charging current measurement (and reduce range to 0 - 200mV for discharge path) or ignore the charging state (SCD and OCD protections for only dishcarge i think) current sensing?
Thanks,
Oğuzhan