Part Number: BQ24172
Finally I selected BQ24172 as the power management IC.
As mentioned by Eric in my previous question, as I do not want to draw current to the system loading (because the loading current is too large for the input power adapter), can I just disconnect the system load from the input source? Please refer to the below picture which is the evaluation board circuit of BQ24172.
Also, as I cut the connection, the input power adapter will not connect to the battery power "Vbat". Can I just short the connection of the FET driven by "BATDRV"?
When I start the system load, if the product is still connecting to the input power adapter, do I need to pull ISET low just like the evaluation board to disable the charging?
If I do not disable the charging while starting the load, is that the IC still drawing current from the power adapter but limited by the charging current (here is 2A), and the battery will supply the remaining power to the load?
Thank you very much!!