Part Number: LM5066I
Other Parts Discussed in Thread: LM5066, LM5066EVK
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM5066I
Other Parts Discussed in Thread: LM5066, LM5066EVK
Hi Ray,
If no devices are displaying then it is very likely a problem with the FTDI driver installed on the PC. Can you try below steps..
1. Terminate the PI-Commander GUI application.
2. Unplug the FT2232h-based host adapter and use the application’s system submenu to un-install the FTDI driver. Go to start menu -> Texas Instruments-> PI Commander ->Advanced -> FTDI -> Uninstall drivers
3. Use the same submenu to install the compatible device driver, which is bundled with the application distribution.
4. Plug in the FT2232h-based host adapter to an available USB port and wait approximately 30 seconds for it to be registered in the system’s device driver tables.
5. Connect the I2C port of the host adapter to the like port of the EVM.
6. Apply the EVM power.
7. Launch the GUI and attempt to communicate with the EVM.
Hope this resolves..
Best Regards,
Rakesh
Thanks Rakesh,
I have tried this several times and each time I am unable to communicate with the EVM. No amount of installs or uninstalls is producing a different result. I have also tried on a separate computer to no avail.
I think the issue is the USB interface adapter that came with the demo kit. Is there another (more reliable) adapter that I can get as a workaround? I really would like to make some progress on my project and the solution out of the box is not working for me.
Ray
I am purchasing a third EVM and a different FTDI connector. Maybe something was dead on arrival.
Maybe something is wrong with my setup, I have 100Ohms connected at the output, Vin is set to 48V, S1 is activated and LM5066 is running drawing 0.48A. See anything amiss here??
The only progress I have made is with another FTDI, it recognizes it as hpa172-0, under that we see an unknown device;
Sure I'll be more than happy to speak with someone to get this board to communicate. Here is my contact information;
rklucik@google.com
I don't know whom to reach out to so if you could put them in touch with me that would be best.
A representative from TI tested an FTDI controller that came with his eval kit and it didn't work. He tried a different FTDI and it worked for him. He then delivered it to my office, I connected it and it started working immediately. I now have access to the development tools!
The issue is the FTDI controllers that you are shipping with the Eval kits. I ordered 3 of them and all 3 were faulty.
Thank you for following up with me and getting me up and running Rakesh.
Best.