Part Number: BQ24253
Other Parts Discussed in Thread: BQ24266, LMR14030, BQ25606
Dear Sir/Madam,
We were using BQ24266 in our circuit, as it is NRND we have replaced the BQ24266 circuit using BQ24253. Attaching the schematic for the battery charger page.
The IC is heating when applied 8.2V@1A, and 8.2V@2A.
L2 Inductor part number is SRP5030CA-1R0M
for testing we have not connected the battery. D+ and D- has not connected as it is not required for our applications. We need stand alone mode not IIC mode. Input 8.2V (+12v identifier name) is fed from LMR14030. But the actual input voltage is changed to +8.2V. Its not 12V.
Please help to identify the heating issue cause.
Regards,
Muthu SVST_Battery Charger.pdf