Part Number: BQ24650
Dear all,
We are working on a device that can be charged at 5V or with solar panel with the BQ24650. We already made a few prototypes in the circuit that we had designed worked correctly charging at 5V 2A.
These days we have ordered the pcb already assembled and our surprise is that the device can no longer charge to 5V. You need 5.3V to 5.5V to start charging.
I have taken captures and made measurements of all parameters and the only difference I have found is here.
The measurement point of the picture in my schematic:
The design is based on BQ24650RVM-639 and we did some changes in VMPPSET=4V and also VBat=4.2V.
Any clue what could happen?
Regards