Part Number: EMB1428Q
Hi Team,
Currently using EMB1428 alone does not match EMB1499.
The circuit diagram is connected as shown in the picture.
Reverse en to the done dir, reverse to DIR _RT three fault angle ground. EMB1428 does not return data when the customer transmits SPI signal 0X01. Set the RST connection to 0, and set the transfer command to 1. This will return the data. What is the role of RST, because it seems that there is no explicit statement in the datasheet.
When the data receives fault[3:0] as 1010 is correct, the switch still cannot be opened. Will it be a problem with Charge Pump? How to resolve this issue?
Thanks.