Part Number: TPS63036
HI TI Team:
The actual test efficiency is lower than that described in the specification,The data are shown in the annex document.
Please help to confirm whether the actual test data is normal ?Where will affected efficiency ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS63036
HI TI Team:
The actual test efficiency is lower than that described in the specification,The data are shown in the annex document.
Please help to confirm whether the actual test data is normal ?Where will affected efficiency ?
Hello,
the efficiency could be worse if an inductor with higher DCR was used.
It also seems that the actual output current and voltage was not measured. This can add further inaccuracy. Note that the output voltage can be up to 6% higher in power safe mode.
I would recommend measuring input and output voltage and current directly at the IC to get reliable results. Also a low DCR inductor should be used.
The typical recommended inductor range from 1 to 2.2uH.
regards,
Julian
Hi Chunqiu,
We haven’t heard back so we're assuming this resolves your issue. If not, just post a reply below, or create a new thread if the thread has locked due to time-out.
As Julian pointed out, check the inductor specifications and also make sure your measurement setup is correct. These application notes might help you:
Measuring efficiency, the right way
Accurately measuring efficiency of ultralow-IQ devices
Calculating and Measuring the No Load Input Current of the Boost Converter
Thanks and regards,
Milos