Part Number: BQ25121A
Hello Team,
I wanted to clarify some operation questions during the following conditions:
This is the setup:
1. Both battery and 5V at IN input are connected.
2. Battery charging is disabled. CD is high.
Open questions:
3. PMID should output IN ?
4. Which source will drive the VSYS BUCK and LDO in the above setup? IN (5V) or Battery?
5. Will the battery have impact on the PMIC operation in this state? It isn’t clear. Are you sure that the IN input (5V) is the supply source in this setup.