Part Number: LM73606
Hi,
I have a design that is from the power designer for 1.2V @ 6A using 18V input, with PG connected to 3.3V and there is a EN voltage of about 5V (PG from previous supply). I use a bias of 3.3V and testing the supply with an electronic load.
When I load it @ 1A the LDO goes from about 3V no load to 3.2V loaded as expected
when I increase the load to 1.5A the LDO drops to about 2.1V and output collapses
I use the same device to produce 3.3V (the one also used as the bias on the 1.2V) and that functions to full 6A using a similar design with values for 3.3V instead of 1.2V (mainly inductor change and feedback) but this uses its output for bias and is auto startup
Any help would much appreciated I need the full current as it is to provide a DDR4 VDDQ
Jessica